This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CC1352R: why is Power consumption of launchpad with FH mode is more than non beacon

Expert 1040 points

Replies: 2

Views: 70

Part Number: CC1352R

Hi,

I am using CC1352 Launchpad for TI 15.4 stack sensor application. I am using FH mode and communicate with collector.

The following are the intervals

1. Polling interval - 5 minutes

2. Reporting interval - 5 minutes

I need low power consumption for my application. With the example code for FH mode my launchpad is giving the following current

Sleep Current - 520 uA

Wake up Current during transmission - 4-8 mA

But in non beacon mode the currents are quite low

Sleep current - 11uA

Active current - 4-8 mA

1. why does this much change is occurring in the FH mode. We would like to use FH mode in our application. If the power consumption is this much high, which will not meet our current requirement

Note: I used all collector and sensor default examples for both FH and NON beacon mode and CC1352 Launchpads

Are anyways are there to reduce the power consumption in FH mode.

2. Broadcast message is been sent from collector to sensor nodes and sensors send broadcast response will the interval can be changed. how does it effects the application?

Thanks and Regards

Haricharan

  • Hi Haricharan,

    What changes have you made inside the Stack to enable FH mode? Please refer to the power suggestions from dev.ti.com/.../frequency-hopping-mode.html

    Also, please note changes to power definitions like described in dev.ti.com/.../example-applications.html

    15.4-STACK-CALC can describe what numbers you should expect when comparing different 15.4-Stack modes. Furthermore, here is an app note on the subject: http://www.ti.com/lit/swra478

    And a relevant E2E post: e2e.ti.com/.../765678

    Regards,
    Ryan

    To better aid the community, please click on the "This Resolved my issue" button whenever a post answers your question!

  • In reply to Ryan Brown1:

    Thanks for quick reply Ryan Brown,
    After removing LEDs and UART enable i am getting 33uA sleep current. With my application i will test and report you back.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.