• Resolved

CCS/LAUNCHXL-CC1310: Collector reading UART cmds

Genius 3205 points

Replies: 10

Views: 141

Part Number: LAUNCHXL-CC1310

Tool/software: Code Composer Studio

Hey guys,

I have a cc1310 Launchpad as collector (collector/sensor example). I've been through UART Echo example and UART.h file reference so far. I can set a HWI at the collector, which sets an event in the collector. When this event is processed in collector.c I want to read the UART line to see if there is some new information.

Here some info regarding the UART line content:

  • There could be no message
  • At the moment, the message is a value between 1-9 however, the length could increase, so I'd like to read until a new line is detected

So far I dont know which settings to use:

  • Callback or blocking?
  • Are readDataMode = Binary and readReurnMode = UART_RETURN_NEWLINE correct?
  • Should I use UART_read? If yes, which arguments should i set?!
  • What further settings should I make?

Kind regards

Slev1n

  • Hey Slev1n,

    Slev1n
    Callback or blocking?

    I would recommend using callback mode so that you don't interrupt application critical tasks during every UART read operation.

    Slev1n
    Are readDataMode = Binary and readReurnMode = UART_RETURN_NEWLINE correct?

    This looks correct.

    Take a look at the UART.h file for more detailed descriptions on settings (also available here).

    Regards,

    Ammar

    Please click the "This Resolved My Issue" button on this post if it answers your question

  • In reply to Ammar N:

    Thank you for your answer Ammar.

    I am currently overwhelmed by the complexity of a simple UART read. The fact that I am quite new to C doesn't make it easier. I will try again to itemize my questions.

    • Is it correct, that the arguments given to read_UART() are automatically passed to the callback function arguments?

    E.g. UART_read(uart_handle, input, 5) causes the callback function to be readCallback(uart_handle, input, 5)

    • I saw some examples posting a semaphore in the callback function. What is this semaphore good for in this case?
    • If I choose to use such a semaphore, do I have to create a new task just for that semaphore?! Would I have to assign the semaphore to the new task ressources?!
    • If I set UART_RETURN_NEWLINE and I set the number of bytes to read to 100 and the message only consists of "1\r\n". Will it just read the 1 and then stop or wait until 100 bytes are reached?!
    • What do I actually have to do in the callback function? Can I just parse the buffer? Would it be enough to write cmd = buffer[0] (i.e. it would be 1 according to my example from above)

    Any help is welcome

  • In reply to Slev1n:

    That is my first try, however the callback functions is never executed.

    char input[255];
    int int_input[5];
    
    void readCallback(UART_Handle handle, void *buffer, size_t num)
    {
        /* Convert char into integer */
        int cmd = input[0] - '0';
        int_input[0] = cmd + 3;
    
    }
    /*
     *  ======== mainThread ========
     */
    void *mainThread(void *arg0)
    {
        char        input;
        const char  echoPrompt[] = "2\r\n";
        UART_Handle uart;
        UART_Params uartParams;
    
        /* Call driver init functions */
        GPIO_init();
        UART_init();
    
        /* Configure the LED pin */
        GPIO_setConfig(Board_GPIO_LED0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
    
        /* Turn on user LED */
        GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_ON);
    
        /* Create a UART with data processing off. */
        UART_Params_init(&uartParams);
        uartParams.writeDataMode = UART_DATA_TEXT;
        uartParams.readDataMode = UART_DATA_TEXT;
        uartParams.readReturnMode = UART_RETURN_NEWLINE;
        uartParams.readMode = UART_MODE_CALLBACK;
        uartParams.readCallback = &readCallback;
        uartParams.readEcho = UART_ECHO_OFF;
        uartParams.baudRate = 115200;
    
        uart = UART_open(Board_UART0, &uartParams);
    
        if (uart == NULL) {
            /* UART_open() failed */
            while (1);
        }
    
        UART_write(uart, echoPrompt, sizeof(echoPrompt));
        int i = 1;
        /* Loop forever echoing */
        while (1) {
            UART_read(uart, &input, 5);
            if (i==1)
            {
                UART_write(uart, &int_input, 5);
                i = 2;
            }
    
        }
    }

  • In reply to Slev1n:

    Hey Slev1n,

    After further investigation, it looks like the use of  UART_DATA_TEXT (consequently UART_RETURN_NEWLINE) is not supported (see https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/489671?CC13XX-UART-RETURN-NEWLINE).

    As your code states, you should enter the callback when your buffer is full. With the following settings, I was able to have the callback entered when the buffer is full.

    /* Create a UART with data processing off. */
    UART_Params_init(&uartParams);
    uartParams.writeDataMode = UART_DATA_BINARY;
    uartParams.readDataMode = UART_DATA_BINARY;
    uartParams.readReturnMode = UART_RETURN_NEWLINE;
    uartParams.readEcho = UART_ECHO_OFF;
    uartParams.baudRate = 115200;
    uartParams.readCallback = &uart0ReadCallback;
    uartParams.readMode = UART_MODE_CALLBACK;

    Remember to increase the size of our buffer (char input[xx];).

    In the callback function, you can parse the full buffer.

    To briefly shed light on your question regarding semaphores: each semaphore pends/posts a specific task. So yes, you'll have to create a task to use the semaphores described in the linked post.

    I recommend taking a look at our Simplelink Academy modules (http://dev.ti.com/tirex/explore/node?a=eCfARaV__2.20.00.38&node=AL.iEm6ATaD6muScZufjlQ__pTTHBmu__LATEST&r=eCfARaV__LATEST&r=eCfARaV__2.40.00.20 ) for more information on TI-RTOS and how to get started.

    Regards,

    Ammar

    Please click the "This Resolved My Issue" button on this post if it answers your question

  • In reply to Ammar N:

    Hey Ammar,

    thank you for your response.

    Regarding the semaphore. Since I am using the sensor collector example, I already have a task with some stack defined and would be able to implement a semaphore, however, I dont think I need one in my application.

    I changed the uart parameter, but still, I the callback function is not entered.

    int int_input[3];
    char input[3];
    const char  echoPrompt[] = "23456789\r\n"; UART_write(uart, echoPrompt, sizeof(echoPrompt)); int i = 1; /* Loop forever echoing */ while (1) { UART_read(uart, &input, 3); if (i==1) { UART_write(uart, &int_input, 3); i = 2; } }

    Still got few questions:

    • Any idea why callback is not entered?
    • Does the callback function wait until the buffer "input" is full?! I dont want to wait until its full, but until the \n is reached in the read string  to enter the callback, because I dont know how long the message will be. or what is UART_RETURN_NEWLINE good for then?!
    • I increased the echoPrompt content to definitely fill the buffer but no success

    Thank you for your help

  • In reply to Slev1n:

    Slev1n
    Does the callback function wait until the buffer "input" is full?! I dont want to wait until its full, but until the \n is reached in the read string  to enter the callback, because I dont know how long the message will be. or what is UART_RETURN_NEWLINE good for then?!

    The callback function should be entered when you send 3 characters through UART (because you've passed in a size of 3 to the UART_read() function). Unfortunately there isn't support for the UART_RETURN_NEWLINE but it is being worked on for future releases.

    In this case, it may be easier for you to read one character at a time. When you enter the callback function, store the character (if it's not the /n char) in a buffer for use by your application. You can add a conditional statement to check if you've received the /n char. 

    Regards,

    Ammar

    Please click the "This Resolved My Issue" button on this post if it answers your question

  • In reply to Ammar N:

    Ah, ok passing only 1 char and then making a conditional statement makes sense. I will try your approach and report back.

    kind regards

    Slev1n

  • In reply to Slev1n:

    The code still does not enter the callback function although I set UART_read(uart, &input, 1). Are my settings correct?!

        /* Create a UART with data processing off. */
        UART_Params_init(&uartParams);
        uartParams.writeDataMode = UART_DATA_BINARY;
        uartParams.readDataMode = UART_DATA_BINARY;
        uartParams.readMode = UART_MODE_CALLBACK;
        uartParams.readCallback = &readCallback;
        uartParams.readEcho = UART_ECHO_OFF;
        uartParams.baudRate = 115200;
    
        uart = UART_open(Board_UART0, &uartParams);
    
        if (uart == NULL) {
            /* UART_open() failed */
            while (1);
        }
            UART_write(uart, echoPrompt, sizeof(echoPrompt));
        /* Loop forever echoing */
        while (1)
        {
            UART_read(uart, &input, 1);
        }
    }

    Besides, I tried parsing the message.

    void readCallback(UART_Handle handle, void *buffer, size_t num)
    {
         if(input == '\n')
        {
            success = true; //set flag that cmd was read completely
            index = 0;
        }
        else
        {
            /* Convert char into integer */
            int cmd = input - '0';
            int_input[index] = cmd + 3;
            index++;
        }
    }
    
    
    

    Is this the right way to parse the message, check if \n is reached and convert a char into an integer?!

    EDIT: I checked the return value of the UART_read function and it is always -1, so I guess there is an error. Any idea what this could mean?! Again, are any settings wrong?

    Does it have anything to do with the fact that I am using a CC1310 launchpad?!

  • In reply to Slev1n:

    Slev1n, At this point I would recommend importing a clean uartecho example and trying again. Your settings are correct, so the callback should get entered. If "input" is not defined as a global, then accessing it in your callback will result in some error. In the uartecho example, "input" is defined inside the main thread, so be sure to exercise caution there.

    Regards,

    Ammar

    Please click the "This Resolved My Issue" button on this post if it answers your question

  • In reply to Ammar N:

    Ok, so I guess besides some of the uart functions not working for the cc1310, it was only my fault that I never entered the callback function. Because I did not read the example correctly or rather misunderstood it. I never entered anything into the putty console, so there was just nothing to read for the uart_read function. Pretty stupid of me, because I thought the written characters of uart_write could be read by uart_read...dont know why I thought that maybe I was confused by all the "echo" stuff.

    However, it does work the way I programmed it and I think I can use it for my approach. If I stumble over something new, I will open a new thread.

    kind regards and thank you for your help Ammar

    Slev1n