Hi
I'm working with CC1101 to receive POCSAG messages (f=452.6MHz, Baud=1200, Ch=25KHz, Dev=4.5KHz).
CC1101 is configured with 2-FSK, FREQ=452.599792MHz, CHANSPC=25.39KHz, DRATE=1.19948kBaud, DEVIATN=4.364KHz, CHANBW=58KHz, FREQ_IF=457KHz, No Preamble/Sync, No CRC, .
RX FIFO and Important Status registers are polled at nearly 4-times the baud rate and sent to a serial port on a PC. During the whole packet reception, RX FIFO=0xFF, FREQEST=0x09, LQI=0x80, RSSI~0xE2 as can be seen below:
| FREQEST | LQI | RSSI | State | PKTS | RXB | RX | 
| 9 | 80 | DE | 0D | E2 | 1 | |
| 9 | 80 | E6 | 0D | E2 | 1 | |
| 9 | 80 | E2 | 0D | E0 | 2 | FF | 
| 9 | 80 | DD | 0D | E2 | 1 | |
| 9 | 80 | E6 | 0D | E2 | 1 | |
| 9 | 80 | E3 | 0D | E0 | 2 | FF | 
| 9 | 80 | E5 | 0D | E2 | 1 | |
| 9 | 80 | E3 | 0D | E2 | 1 | |
| 9 | 80 | E6 | 0D | E0 | 2 | FF | 
| 9 | 80 | E2 | 0D | E2 | 1 | |
| 9 | 80 | E4 | 0D | E2 | 1 | |
| 9 | 80 | E1 | 0D | E2 | 2 | FF | 
What's the problem with the data? Which configuration is wrong?
Thank you in advance