This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Excel sheet to estimate range for Indoor and Outdoor

Genius 16850 points

Replies: 80

Views: 102036

Hi,

The attached excel sheet helps to estimate a practical range estimation for indoor and outdoor radio links.

The outdoor is based upon Line-of-Sight (LOS). For the indoor estimation, construction materials can be selected that are between the Tx and Rx unit. The greater the attenuation of the combined material between the Tx and Rx unit, the shorter the distance.

This has been used a lot in TI seminars and is a helpful tool for calculating a realistic and conservative range expectation.

The latest version is available at: http://www.ti.com/tool/rf-range-estimator

Latest version (1.17) has been updated to include:

  • CC2640R2F - 500 kbps (BLE)
  • CC2640R2F - 125 kbps (BLE)

Any feedback is welcomed.

Regards, Richard

 

80 Replies

  • Good work Richard

  • Hi,

    What version of Excel should be used for this sheet? It seems I do not have any options to select in some cells. I use Excel 2007, macros are allowed.

    Screenshot is attached.

  • Genius 16850 points

    In reply to Oleg Pushkarev:

    Range Estimation for Indoor and Outdoor Rev1_06 - Excel 97-2003 version.xls

    Hi,

    The version is Microsoft Excel 2010. Attached is an Excel 97 - 2003 version. Let me know if this solves the issues.

    Regards, Richard

     

  • In reply to RGW:

    It seems I see the same result (wrong one) . Could you post screenshot of this Excel Sheet as it works on your PC and provide brief comments - which cells could be modified by customer?
    Br,
    Oleg
  • Genius 16850 points

    In reply to Oleg Pushkarev:

    Hi,

    there will be an app note released soon that describes all the parameters in this excel calculation. All the grey zones are input fields which can be selected via drop down menus or by just entering a value.

     

  • Genius 16850 points

    In reply to RGW:

    The fields that are shown in grey are the input fields. The heights of the Tx antenna (h1) and Rx antenna (h2) are entered at the top; for hand-held devices this is typically in the region of 1.2 m. The scaling of the graph is just for the figure scale shown on the right hand side and this is flagged in red if the scale is less than the calculated range for Friis and the ground model (2-ray). The frequency field is the operating frequency of the radio. For the signal polarity, “V” for vertical polariztion and “H” for horizontal polarization can be entered. The conducted transmitted output power should then be entered and this is normally between -20 dBm to +30 dBm pending the radio solution. The gain for the Tx antenna (GT) and Rx antenna (GR) must be entered; for a perfect matched dipole this is 2.1 dB, if this is unknown keep this value between 0 dB and 2.1 dB. There is a list of antennas which can be chosen with a recommended value for the gain; the gain in the list varies from -6 dB to +2.1 dB. The surface (εr) shown in figure 1 can be set between Ground (εr = 18), Water (εr = 88) and Sand (εr = 2.5); if this is unkown then keep this at a typcial value of 18.

     

    For the sensitivity level of the radio, a list is available of the various radios and the data rate settings. The data rate setting is important since this determines the actual senisitivty level of the radio for a particular date rate. A larger data rate will always have a lower sensitivity level (-174 dBm + 10log10(BW) ).

     

    Bandwidth (BW)

    Theoretical sensitivity level

    1 Hz

    -174 dBm

    1 kHz

    -144 dBm

    1 MHz

    -114 dBm

    Sensitivity level decreasing with increasing bandwidth

     

    The list of radios with data rates supported in the excel ver1.06 release is shown in Table x. If a specific radio and data rate cannot be found then choose a setting that gives the same sensitivity level that is specified in the data sheet.

     

    Sub-1 GHz Devices

    Sensitivity level (dBm)

    2.4 GHz Devices

    Sensitivity level (dBm)

    CC11L - 0.6 kbps

    -116

    CC2520 - 250 kbps

    -98

    CC11L - 1.2 kbps

    -112

    CC2530 - 250 kbps

    -97

    CC11L - 38.2 kbps

    -104

    CC2538 - 250 kbps

    -97

    CC11L - 250 kbps

    -95

    CC2540 - 1 Mbps (HG)

    -93

    CC11L - 500 kbps (MSK)

    -90

    CC2540 - 1 Mbps (Std)

    -87

    CC11L - 500 kbps (4-FSK)

    -96

    CC2541 - 250 kbps (160 kHz fdev)

    -98

    CC110x - 0.6 kbps

    -116

    CC2541 - 500 kbps (MSK)

    -99

    CC110x - 1.2 kbps

    -112

    CC2541 - 1 Mbps (160 kHz fdev)

    -91

    CC110x - 38.2 kbps

    -104

    CC2541 - 1 Mbps (250 kHz fdev)

    -94

    CC110x - 250 kbps

    -95

    CC2541 - 2 Mbps (320 kHz fdev)

    -86

    CC110x - 500 kbps (MSK)

    -90

    CC2541 - 2 Mbps (500 kHz fdev)

    -90

    CC110x - 500 kbps (4-FSK)

    -96

    CC2543 - 250 kbps (160 kHz fdev)

    -98

    CC111x - 1.2 kbps

    -110

    CC2543 - 500 kbps (MSK)

    -98

    CC111x - 38.2 kbps

    -102

    CC2543 - 1 Mbps (160 kHz fdev)

    -91

    CC111x - 250 kbps

    -94

    CC2543 - 1 Mbps (250 kHz fdev)

    -94

    CC111x - 500 kbps (MSK)

    -86

    CC2543 - 2 Mbps (320 kHz fdev)

    -86

    CC1125 CC1190 - 0.6 kbps (LRM)

    -129

    CC2543 - 2 Mbps (500 kHz fdev)

    -90

    CC1120 CC1190 - 0.6 kbps (LRM)

    -126.5

    CC2544 - 250 kbps (160 kHz fdev)

    -95

    CC112x - 0.3 kbps (CG - 4 kHz fdev)

    -127

    CC2544 - 500 kbps (MSK)

    -96

    CC112x - 1.2 kbps (4 kHz fdev)

    -123

    CC2544 - 1 Mbps (160 kHz fdev)

    -87

    CC112x - 1.2 kbps (10 kHz fdev)

    -120

    CC2544 - 1 Mbps (250 kHz fdev)

    -91

    CC112x - 1.2 kbps (20 kHz fdev)

    -117

    CC2544 - 2 Mbps (320 kHz fdev)

    -84

    CC112x - 4.8 kbps (OOK)

    -114

    CC2544 - 2 Mbps (500 kHz fdev)

    -88

    CC112x - 38.4 kbps (20 kHz fdev)

    -110

    CC2545 - 250 kbps (160 kHz fdev)

    -98

    CC112x - 50 kbps (25 kHz fdev)

    -110

    CC2545 - 500 kbps (MSK)

    -98

    CC112x - 200 kbps (83 kHz fdev)

    -103

    CC2545 - 1 Mbps (160 kHz fdev)

    -91

    CC120x - 1.2 kbps (4 kHz fdev)

    -122

    CC2545 - 1 Mbps (250 kHz fdev)

    -94

    CC120x - 4.8 kbps (OOK)

    -113

    CC2545 - 2 Mbps (320 kHz fdev)

    -86

    CC120x - 32.768 kbps (50 kHz fdev)

    -108

    CC2545 - 2 Mbps (500 kHz fdev)

    -90

    CC120x - 38.4 kbps (20 kHz fdev)

    -110

    CC2500 - 2.4 kbps

    -104

    CC120x - 50 kbps (25 kHz fdev)

    -109

    CC2500 - 10 kbps

    -99

    CC120x - 100 kbps (50 kHz fdev)

    -107

    CC2500 - 250 kbps

    -89

    CC120x - 500 kbps (MSK)

    -97

    CC2500 - 500 kbps

    -83

    CC120x - 1000 kbps (4-GFSK)

    -97

    CC251x - 2.4 kbps

    -103

     

     

    CC251x - 10 kbps

    -98

     

     

    CC251x - 250 kbps

    -90

     

     

    CC251x - 500 kbps

    -82

    Table x. Sub-1 GHz and 2.4 GHz Devices Sensitivity Levels for various data rates

     

    The input field selection for “Select Effective Attenuation between Rx and Tx” contains a number of options which take into account the size of the guard band (link margin); and several input fields to select various construction materials normally used for indoor range prediction. The level of the guard band depends on the level of margin that is required. Theoretically, this can still be 0 dB and the radio link will still work. However, a certain guard band should be taken and this is normally in the range of 10 dB to 20 dB. For a system that requires a strong and reliable “fail safe” RF link then the margin could be increased furthermore. Similarly, for a system that can accept re-transmissions and temporary link losses then this can be reduced. With multi-path propagation effects, the signal level can vary up to 15 dB so having a guard band > 15 dB will take this into account. When not using antenna diversity then the recommended guard band is 20 dB and with antenna diversity this can be reduced to 10 dB guard band.

     

    When calculating outdoor Line-of-Sight (LOS) range then “LOS” can be selected for the three input field options as can be seen in Figure tbd. For improved indoor range estimation, various construction materials can be chosen for the three input field options, the choice of material is shown in Table x.

     

    Construction

    Material

    Attenuation (dB)

    500 MHz

    Attenuation (dB)

    1 GHz

    Attenuation (dB)

    2.4 GHz

    LOS

    0

    0

    0

    7" brick

    3.5

    5.5

    7.5

    8" concrete

    21

    25

    32

    1/2" drywall

    0.1

    0.3

    0.6

    1/2" glass

    1.2

    2.2

    3.4

    4" reinforced concrete

    23

    27

    31

    3" lumber

    1.5

    3

    4.7

    Table xy. Typical attenuation for various construction materials at 500 MHz, 1 GHz and 2.4 GHz

     

    As can be seen in Table x, the material penetration is highly frequency dependent and the advantages of operating at a lower frequency is clearly seen in the link budget and range expectation. A rule-of-thumb is every 6 dB increase in a link budget doubles the range distance. To send a signal through an 8” concrete wall at 1 GHz will have approximately twice the range compared to a similar system operating at 2.4 GHz.

     

    When all the parameters with the height of the antennas, frequency, polarization, output power, antenna gain, ground surface, sensitivity level, guard band and material between Rx & Tx; then a more realistic range can be calculated compared to the standard Friis formula.

     

  • Genius 16850 points

    In reply to RGW:

    Ver 1.07 supports CC13xx and CC26xx.

     

  • great work indeed.

    signature

  • Genius 16850 points

    In reply to Harry:

    Documentation on how to use this excel range calculation can be found at: www.ti.com/.../swra479

    Regards, Richard

     

  • In reply to RGW:

    very timely!

    signature

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.