This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310 to CC1350 Fails

Other Parts Discussed in Thread: CC1350, CC1310

Dear Support:

I downloaded the SDK for the TI-15.4 stack v2.0.0.25.  I noticed that the projects are built for the CC1310.  However when I go to the properties for the project and change the device to the CC1350F128 for the CC1350 launchpad that it fails during the linking stage with the following message using CCS:

<Linking>

 

undefined first referenced

  symbol       in file    

 --------- ----------------

heapEnd   <whole-program>

 heapStart <whole-program>

 

error #10234-D: unresolved symbols remain

error #10010: errors encountered during linking; "coprocessor_cc13xx_lp.out" not built

gmake: *** [coprocessor_cc13xx_lp.out] Error 1

 

>> Compilation failure

makefile:176: recipe for target 'coprocessor_cc13xx_lp.out' failed

gmake: Target 'all' not remade because of errors.

 

**** Build Finished ****

And then when I try to go back and select the CC1310 that it fails also with the same message.  The only way I found to recover is to delete the project and go back to the original version in order to be able to build again using the CC1310.  Do you know what is the problem?  Please advise.

Thanks,
Tim