Goodmorning,
I'm developing a board involving the cc1310 7x7 4 layer.
I would know some information:
1)Are there any other (more recent) design files in addition to "SimpleLink CC1310 4-Layer 7x7 Differential 779-930 MHz v1.0.1 Design Files"?
2)Are there any design files whit Balun integrated in the RF path.
3)The files that you provide (SimpleLink CC1310 4-Layer 7x7 Differential 779-930) have to be opened with Cadence Allegro suite, but I need Altium Design files. I know that is possible to import them, but to do that it is necessary to have both software installed (so expensive).
4) Are there some detailed pdf files or similar with precise hardware and PCB design guidelines to include the CC1310 in a personal board project?
Thank you very much for the attention and the help.
Best regards
ST