Part Number: CC1310
I've been playing with SmartRF studio and testing the performance of the CC1310. SmartRF studio has an option for Long Range mode. I need details of what long range mode is!!!
I think its called fecMode in the formateConf register. FEC mode talks about Manchester encoding.
Also the Symbol rate is divided by 16 to get the data rate, add on the Manchester encoding and the duration of the transmission can be calculated.
SmartRF studio also does not appear to allow packet data length to be changed in "long range mode"
More detail on the operation of Long range mode is required. I've dug around looking to reference to long range mode but could find nothing.
Any apps notes, etc would be great.
Thanks,
Greg