Hello,
I have tested with CC1120DK (TrxEB+CC1120EMK).
- SmartRF Studio Setting : Generic 434Mhz / Bit rate:1.2kbps, 4-GFSK, RX BW : 25 kHz (434)
I have only changed 2-FSK to 4-GFSK on default setting.
If the specific repeated characters('aaaaaaaaaaaaaaaaaaaaaaaa') trasmited, the CRC error was occured.
1. Random data trasmit --> CRC is OK
2. Text data('aaaaaaaaaaaaaaaaaaaaaaaa') trasmit --> CRC error
3. Text data('aaaaaaaaaaaaaaaaaaaaaaaa') with Whitining option trasmit --> CRC is OK.
If the modulation was set with 2-FSK or 2-GFSK, there was no problem.
But, if specific repeated characters('aaaaaaaaaaaaaaaaaaaaaaaa') was transmited with 4-FSK or 4GFSK modulation, the CRC error was occured.
Must we use Whitening option on 4GFSK modulation ?
Could you please explain cause of error and about Whitening option?
Thanks.