This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Does WOR on the CC1310 work in Long Range mode?

Expert 1595 points

Part Number: CC1310

Hi all,

At the while I have been trying out the WOR examples on the CC1310 launchpad using 50 kbps,2-GFSK, 25kHz deviation @433Mhz. Just wondering if WOR will work for other settings such as 5 kbps SimpleLink Long Range or 2.5 kbps SimpleLink Long Range? Does it mean that the range will be longer if I use either of these Long Range settings, even if I use the same antenna and tx power?

Thanks!

  • Hi,

    For SimpleLink Long Range Mode, a time-synchronous approach is preferred. All nodes in a network would use a common time-base and wake-up in predefined slots. Use either TI 15.4 stack if you want a comprehensive solution or have a look at the Synchronous Packet example if you want to use the raw proprietary API. You can also send  and receive packets with EasyLink using synchronous timing which is much simpler.

    Background: It does usually not make sense to implement a Wake-on-Radio scheme with the SimpleLink Long Range Mode.  In this mode, it is possible to recover a signal even from below the noise floor (the noise floor is quite high in many regions). On the Gen-FSK PHY, we use RSSI measurement and preamble quality check to quickly determine a signal on the air after wake-up. Both techniques are useless for SimpleLink Long Range mode if the signal level is below the noise floor.

  • Hi Richard,

    Thank you for the information. My application involves multiple transmitters and receivers. The transmitters send its MAC address in the packet and the receivers have a white list of MAC addresses. Transmission occurs randomly, 20 times a day.

    Both the transmitters and receivers run on batteries. I am just wondering whats the current consumption between WOR and synchronous timing? I presume WOR will be more suitable for my application since I am not transmitting at regular intervals.

    With WOR and using 50 kbps,2-GFSK, 25kHz deviation @433Mhz, I wonder if it is possible to achieve a max 200m distance if both side are using PCB trace antennas
  • Kian said:

    Both the transmitters and receivers run on batteries. I am just wondering whats the current consumption between WOR and synchronous timing? I presume WOR will be more suitable for my application since I am not transmitting at regular intervals.

    This can not be said in a general manner. There are many things to consider:

    • Wake-on-Radio uses a simple system design with a very long preamble to make nodes catching a signal. When any node finds the preamble on the air, it will stay awake and try to receive the message until the address filter stops reception.
    • You need to wake up often enough to not miss a packet
    • The preamble needs to match the wake-up interval. But the longer the interval, the higher the utilization of the channel. Not only might this violate regulations, but means also that you waste a lot of channel space for preambles.

    With synchronous timing, the channels can be used much more efficiently, but the system design is trickier. We don't have any collaterals/guides for the system design and so don't we provide information on power consumption unfortunately. For wake-on-radio, you could measure our wake-on-radio example and then extrapolate that calculation to your system design taking above points into consideration.

    Kian said:
    With WOR and using 50 kbps,2-GFSK, 25kHz deviation @433Mhz, I wonder if it is possible to achieve a max 200m distance if both side are using PCB trace antennas

    With nothing in between, yes. With a lot of steel and concrete in between, maybe. I suggest to take a launchpad and check. There is a 433 Mhz CC1310 launchpad out now.

  • Note that the PCB antenna on the www.ti.com/.../launchxl-cc1350-4 has poor efficiency and should only be used for functional testing. For range testing use an external antenna. Note that an efficient PCB @433 MHz is large.