Other Parts Discussed in Thread: CC1101, CC1120, CC1190
Hi,
I have a TrxEB and CC1101_CC1190EM 868Mhz 2.1. I have configured the TrxEb to work with CC1120 and selected the PER test. The range which I see is about 200m, beyond which the PER is 100%.
Under the same conditions, when I connect the CC1120 with TrxEB, i get a range of about 900m.
CC1190 is supposed to have higher Tx power and better sensitivity so can expect a higher range but Its not seen to be so..