Hi All,
Met another issue with CC1125. I am using CC1125 as core device in a data link device and need to meet ETSI 300 113 spec. But the Rx selectivity is way lower than spec. Below is the configuration.
Modulation: 4GFSK
Symbol rate: 7.6K
Modulation Dev: 3.4K
this configuration is used for 25KHz channel that requires 70dBc adjacent channel selectivity for receiver per ETSI 300 113 standard, but what I measured is only 52dB. The circuitry has no external crystal or saw filter as channel filter in that impossible to find an appropriate 25KHz filter at UHF or 800MHz band. The selectivity is mostly due to the receiver backend CC1125 so some questions raised as below:
According to CC1125 datasheet, I found that it seems can only achieve 57dB selectivity.
Question is:
1. If the CC1125 is been limited internally on the selectivity performance, due to internal ADC resolution or digital filter limitations.
2. Is there any method to improve it ?
Used to meet some Tx transient spurious issue on the CC1125 and now we are little struggling on the receiver selectivity. If CC1125 cannot meet 70dB spec then we have to give it up and moving to new candidates or new receiver architecture.
Any one has same experience or any idea may help.
Thanks