Part Number: CC1310
Hello,
A fatal problem was found after using the CC1310. Questions are as follows:
1)When the TCK interface in the JTAG interface of the CC1310 is interfered, the CC1310 can easily enter the Debug mode. At this time, the chip must pass PIN-RESET and power down in order to return to normal.
2)The pull-up resistor provided by the datasheet does not completely avoid interference. Therefore, whenever the CC1310 performs a software reset, it has a certain probability of entering the Debug mode during use, causing the chip to fail to work properly.
3)Debug mode: When TCK receives the interference, it will set HIB FLAG high and enter the debug mode after the next software reset. However, we cannot guarantee that TCK is disturbed. If there is a way to reset it, clear the HIB FLAG by software?
thanks.