Hello all,
I have a question related to CC1310 used with CoProcessor code. We are developing wearable device in which we use cc1310 as wireless communication module. WE have a base station which collects data from up to 30 remote units. Our base station is single board computer running ubuntu and has cc1310 module connected to it via uart and we use the linux gateway example to collect the data and setup the cc1310 module. On our remote units we have also MCU connected with uart to cc1310 module and we are going to use the CoProcessor code on the cc1310. So our remote units are sensors and my question is how to configure the cc1310 Coprocessor module to act as a sensor (connect and send data to the linux gateway). Can someone tell me the configuration command sequence which has to be performed in order to setup the cc1310 to connect to our gateway and send data to it? Also is there any example available on how to use the Coprocessor as a sensor node not as a collector node.
Thank you in advance!
Best regards,
Ivan