Other Parts Discussed in Thread: CC1101, , CC1070
Hi,
I have a requirement for a legacy transmit only RF project. Previously a CC1101 in asynchronous transfer mode
"Asynchronous transfer is included in the CC1101 for backward compatibility with systems that are already using the asynchronous data transfer"
The CC1101 would have it's GDO pin placed into asynchronous serial mode/direct mode which would allow a high or low data input on the GDO to control the TX signal. This is done manually at a data rate of 33.3khz.
The receiver hardware will not change but must support the CC1310 operating in the equivalent mode.
Would this be possible on the CC1310?
Kind Regards,
Scot