Part Number: CC1310
Hi All,
My test hardware is CC1350-4 Launchpad, I want to test the frequency setting of 420 to 430 Mhz.
When I use SmartRF studio7, If set to 430 Mhz, it will display a warning color in the frequency field, but the radio still worked.
If the frequency setting is lower than 429Mhz, the radio does not work.
After check the settings on smartRF studio, the IoDivider is different. Is there any override command should add to the settings?
BR,
Jack