Hi,
I have flashed devices according to project 0. They connect and it's working. I use packet sniffer and wireshark to monitor the packets.
Then I do a factory reset on the sensor. Then I activate permit join on collector. I can see in wireshark that the association process is taking place just after I activate permit join on the collector. I also notice through wireshark that the long addresses are exchanged so that the same physical sensor is recognized as the original device that originally was associated with the collector the first time - great! Then the sensor data (the very long payload) is transmitting regularly (seen from wireshark). I can even toggle the LED sensor through the collector. However: The collector UART output is stating "!Responding: 0x1" for a very long time (10 minutes etc), and then suddenly the sensor data is output on the UART eventually. It seems that there is something wrong here... The collector is evidently receiving the sensor data, but the "top layer" code does not seem to know this.
Let me know if you can reproduce this. Thanks.
HC