Part Number: CC1310
Hello,
we want to use the SPI Slave mode of the CC1310 device.
But we can't receive any packet.
If we use SPI Master mode, everything is fine.
So i think the IO Port definition and initialisation of the SPI is OK.
The external Master send a packet with 32 Bytes and 0,75 Mbit, but we never seen a callback ...
Our Code
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <string.h>
/* Driver Header files */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/SPI.h>
#include <ti/display/Display.h>
/* Example/Board Header files */
#include "Board.h"
#define SPI_MSG_LENGTH (32)
#define SLAVE_MSG ("Hello from slave, msg#: ")
#define MAX_LOOP (10)
unsigned char slaveRxBuffer[SPI_MSG_LENGTH];
unsigned char slaveTxBuffer[SPI_MSG_LENGTH];
unsigned char txSPIBuf[SPI_MSG_LENGTH];
unsigned char rxSPIBuf[SPI_MSG_LENGTH];
#define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0)
bool Received = false;
void transferCallback(SPI_Handle handle, SPI_Transaction *transaction)
{
Received = true;
}
#define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0)
void Test(void)
{
SPI_Handle handle;
SPI_Params params;
SPI_Transaction transaction;
bool transferOK;
uint8_t Buffer[SPI_MSG_LENGTH];
uint8_t i;
SPI_init();
SPI_Params_init(¶ms);
params.bitRate = 1000000; // Maximum bit rate as slave
params.frameFormat = SPI_POL0_PHA1;
params.mode = SPI_SLAVE;
// params.mode = SPI_MASTER;
params.transferMode = SPI_MODE_CALLBACK;
params.dataSize = 8;
params.transferCallbackFxn = transferCallback;
/********************************************
* Configure the transaction
********************************************/
transaction.count = SPI_MSG_LENGTH;
transaction.txBuf = (void *) txSPIBuf;
transaction.rxBuf = (void *) rxSPIBuf;
/********************************************
* Open the SPI and initiate the first transfer
********************************************/
handle = SPI_open(Board_SPI0, ¶ms);
/********************************************
* Start and wait for Master CLK
********************************************/
SPI_transfer(handle, &transaction);
// SPI_control(handle, SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE, NULL);
strncpy((char *) txSPIBuf, SLAVE_MSG, SPI_MSG_LENGTH);
while (1)
{
if (Received == true)
{
transferOK = SPI_transfer(handle, &transaction);
for (i = 0; i < SPI_MSG_LENGTH; i++)
Buffer[i] = rxSPIBuf[i];
Received = false;
i = 1 ;
txSPIBuf[sizeof(SLAVE_MSG) - 1] = (i % 10) + '0';
memset((void *) rxSPIBuf, 0, SPI_MSG_LENGTH);
transaction.count = SPI_MSG_LENGTH;
transaction.txBuf = (void *) txSPIBuf;
transaction.rxBuf = (void *) rxSPIBuf;
}
}
}
regards Andreas