This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC1310: Debugging in Code Composer studio Contiki CC1310 launchpad Project Hangs

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310

Tool/software: Code Composer Studio

Hi

I was successfully able to build the contiki CC1310 launchpad project using the steps mentioned in the pptx "Contiki and Code Composer Studio". When I was debugging step by step code gets hang at the line 93 in the contiki-main.c file LOG_INFO("Starting " CONTIKI_VERSION_STRING "\n");


I dont understand which console in code composer studion we can see the output. Also while debugging it is not moving forward.

Is there configuration to be done for this .

Please help me out in this regard

Thanks 

Safvan