Other Parts Discussed in Thread: BLE-STACK, , CC2540, CC2640
Tool/software: TI-RTOS
Can someone explain the following parameters in gap.h?
typedef struct { uint16_t connectionHandle; //!< Connection handle of the update uint16_t intervalMin; //!< Minimum Connection Interval uint16_t intervalMax; //!< Maximum Connection Interval uint16_t connLatency; //!< Connection Latency uint16_t connTimeout; //!< Connection Timeout uint8_t signalIdentifier; //!< L2CAP Signal Identifier. Must be 0 for LL Update } gapUpdateLinkParamReq_t;
The documentation is a bit useless, especially regarding the interval and conn parameters (as you can see).