Hi
According to EN 50131-5-3 standard , in order to meet Grade 3 Sub 1GHz security system it needs Transceiver with Dual band support (like 868 and 433 MHz).Right?
The questions about Dual band implementation in CC1310 is as follow:
- Does CC1310 meet EN 50131-5-3 Grade 3? What needs for that?
- Could CC1310 transmit & receiving in two separate bands such as 868 and 433 to overcoming the interfering signals (Immunity to interference section 4.4 of EN 50131-5-3 ------> 10v/m)?
- Which selectivity required from our line up receiver (external SAW filter) to meet immunity to interference requirement 10v/m?
Regards
Roni