Tool/software: TI-RTOS
Hi,
I'm developing an application based on the sensor and coordinator beacon example.
My config:
* APIMAC_GENERIC_ETSI_863_PHY_133 (200 kbps)
* Beacon order: 7 (614 ms interval);
* Superframe order: 7;
* Reporting interval: 100 ms;
* Polling interval: 10 minutes(Is big because I only send 1 byte of information from the coordinator and I send in the beacon payload);
I am reporting with an interval of 100ms and polling with an interval of 10 minutes and some times the Sensor_sendMsg fails a few times(4-6 typically) sequentially. I'm using only one sensor to don't get collisions. Any idea why this happens? In what cases the Sensor_sendMsg return false?
Best regards,