Other Parts Discussed in Thread: CC1310
I imported the rfPacketErrorRate code into code composer this is the code http://dev.ti.com/tirex/explore/node?node=AAH5pdKIQF7AwxOZbakjeg__eCfARaV__LATEST . Successfully built it and initiated the CCS debugger V9.01 for CC1310 launchpad. Stepping through the code quickly ran into what appears to be no source code for power_init. I included it, or include ti/drivers/power/PowerCC26XX.c and .h. So I then built and stepped through the code further. But, I then get a second missing source. This time I was not able to find the source anywhere either in the code composer update choices or in the CC1310, CC26xx SDK. Here is the error print from the CCS debugger.
"Can't find a source file at "/db/vtree/library/trees/mcpi/mcpi-4.10.01.00/exports/coresdk_cc13xx_cc26xx_4_10_01_00/kernel/nortos/dpl/ClockPTimer_nortos.c"
Locate the file or edit the source lookup path to include its location."
I tried using the ClockPTimer_nortos.c under simplelink_cc13x0_sdk_3_10_00_11/kernel/nortos/dpl directory but this code with a few includes added, does not build. Has a lot of errors. It seems I am looking for directory coresdk_cc13xx_cc26xx_4_10_01_00 that probably was used at TI but not available for release. I see that builder is looking for source under /db directory, I used to work at TI so I know those are local disk partitions inside the company. Apparently the code is dependent on these in order to see pockets of source code, perhaps as the code evolved since the CC1310 was developed. The code did build with binary replacing some of the source and I did disconnect the board after loading it and was successful at running rf packet transmission and receive between 2 boards with no packet errors, The downloaded code has more menu choices with that appear to be CC26XX related.
Any advice appreciated on what to do about locating the portable, full source code for the CC1310 launch pad for this demo. Thanks.