Other Parts Discussed in Thread: CC1310, CC1350
Tool/software: TI-RTOS
Hello All,
I wanted to implement FACTORY RESET on our CC1310 device. I'm planning to add this on the offchip_bim example.
My idea is to check if a certain location on the external flash (preferably the address for BLE STACK) contains an image.
If it doesn't contain an image, will copy the image from the internal flash into the external flash.
However, I can't find any function that could read from the internal flash on file flash.c (C:/ti/<sdk_version>/source/ti/device/cc13x0/driverlib).
There is a HalReadFlash function on the hal_flash_wrapper.c (C:/ti/<sdk_version>/source/ti/ti154stack/hal/src/target/_common)
but can't compile the code successfully when I add it on my application code.
Any help would be appreciated.
Anyways, below is my setup:
CCS version: 8.3.1
SDK version: 2.20.00.38
Thanks and Regards,
Elton