Other Parts Discussed in Thread: CC1310
Hi,
1. I have a border router with SPSGRF-915 (from ST) sitting on a Linux board (that Linux board is working as a gateway but actually does many more thing than just gateway), border router microcontroller running https://github.com/contiki-os/contiki/tree/master/examples/ipv6/rpl-border-router code.
2. Now, we are developing node with TI CC1310 (it was initially based on ST microcontroller and SPSGRF-915, but nodes are in very high volume and to reduce cost, our team decided to switch to CC1310).
3. I am running https://github.com/contiki-os/contiki/blob/master/examples/er-rest-example/er-example-server.c code on CC1310 launch pad.
Issue: No communication between the border router and TI CC1310 node
What I did so far;
4. Changed RDC and made same as border router
#define NETSTACK_CONF_RDC nullrdc_driver
5. Changed RF channel same as border router
#define RF_CORE_CONF_CHANNEL 0
6. Using prop mode on CC1310
#define NETSTACK_CONF_RADIO prop_mode_driver
I did that by defining #define CPU_FAMILY_CC13XX 1 in contiki-conf.h,
7. Changed to 915MHz, same as border router
/* Default band selection to band 4 - 863MHz */ #ifdef DOT_15_4G_CONF_FREQUENCY_BAND_ID #define DOT_15_4G_FREQUENCY_BAND_ID DOT_15_4G_CONF_FREQUENCY_BAND_ID #else #define DOT_15_4G_FREQUENCY_BAND_ID DOT_15_4G_FREQUENCY_BAND_915 #endif
What else should I change? And also, how IPV6 address is forming, I mean which .c file taking care of that? Please help me with that, I have almost spent a week with no success. Thanks!
-Anesh