Part Number: 430BOOST-CC110L
I just purchased one 430BOOST-CC110L plus two MSP430G2ET Launchpads to test 915MHz Wireless transmission between MSP430 devices. Both of the MSP430G2ET kits were tested and worked in their original configuration.
Then I replaced both MSP430G2533 micros with those contained in the 430BOOST-CC110L kit, installed the two Anaren modules as shown in the instructions. The instructions about the UART jumper placement was confusing since neither drawing was for the MSP430G2ET board - I tried the straight jumpers and the crossover jumpers. My problem is the Anaren ATC Booster Stack Lite program is completely blank (no data received). The MSP430G2ET Green and Yellow LEDs are ON (USB interface LEDs). Both MSP430G2ET boards give the same result [blank data, plus greyed out sections of the screen].