We have been using the chip for many years and on many markets/frequencies. The normal operation in this application is that the chip is in sleep mode, when it wakes up to make a transmission there are mainly 2 problems:
When sending the STX (Start Transmission) command, it sometimes happens that the transmission doesn' start. I have improved this by checking that the ichip s actually transmitiing, if not I send the STX command again, this have improved the situation. Are there some other work-around for this?
The equipment is for indoor use. On some chips the self calibration doesn't work properly. I have used test FW that recalibrates the PLL every 10th second. The chip can work fine for hours. Sometimes the self calibration starts to fail (no PLL lock, checked in the registers). When this happens, it fails all times for minutes, then it's OK for a whila again. Since the equipment is for indoor use, the recalibration should not be required (+-40C is the limits according to the data sheet, chapter 22.1). Since the recalibration is not really needed, is it OK to calibrate the chip once, save the contents of FSCAL1-3 and use these calibration values (from chapter 28.2). The FSCAL values have to be collected for the actual frequency). Is this a good route? Any other suggestions?
Mats Q