This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1350: Porting project from contiki 3.0 to contiki-ng cc1350

Part Number: LAUNCHXL-CC1350
Other Parts Discussed in Thread: CC1350

Hi all

I wanna porting my firmware based on contiki 3.0  in contiki-ng. I tried to compile but it doesnt' work. It appears: No rule to make a target.

How can I do ?

Best Regards

Francesco

  • Hi toby,

    thanks for your fast reply. I tried to write this command but It appears: No rule to make a target

     make TARGET= cc26x0-cc13x0 BOARD=launchpad/cc1350 MTX_DOME.bin

    where MTX_DOME is a folder which contains my project

    Which is the problem?

    Best

    Francesco

  • You are not supposed to write "MTX_DOME.bin" as the target.

    Simply call

    make TARGET= cc26x0-cc13x0 BOARD=launchpad/cc1350 

  • I tried but It appears always same error: no rule to make a target. I think the makefile is different between contiki 3.0 and contiki-ng. 

    Which makefile do I have to change ? Or the problem is another ?

    Thanks 

     Francesco 

  • I recommend you to read the online wiki for Contiki-NG: github.com/.../The-Contiki‐NG-build-system

  • Part Number: CC1350

    I wanna compile my project in contiki ng and I modified this makefile because my project was in contiki 3.0

    Hi thanks for fast reply this is makefile about platform:

    C:\cygwin64\home\user\contiki-ng-mtx\arch\platform\cc26x0-cc13x0\launchpad:

    CFLAGS += -DBOARD_LAUNCHPAD=1

    CONTIKI_TARGET_DIRS += MTX_launchpad common

    BOARD_SOURCEFILES += board.c launchpad-sensors.c leds-arch.c button-sensor.c
    BOARD_SOURCEFILES += ext-flash.c board-spi.c
    MODULES += arch/dev/ext-flash

    ### Signal that we can be programmed with cc2538-bsl
    BOARD_SUPPORTS_BSL=1

    BOARD_SOURCEFILES += sensortag-sensors.c sensor-common.c
    BOARD_SOURCEFILES += bmp-280-sensor.c tmp-007-sensor.c opt-3001-sensor.c
    BOARD_SOURCEFILES += hdc-1000-sensor.c mpu-9250-sensor.c button-sensor.c

    BOARD_SOURCEFILES += reed-relay.c ext-flash.c buzzer.c

    BOARD_SOURCEFILES += board.c board-spi.c board-i2c.c

    This is contained in this path: C:\cygwin64\home\user\contiki-ng-mtx\arch\platform\cc26x0-cc13x0\MTX_launchpad\cc1350

    ### Will allow the inclusion of the correct CPU makefile
    CPU_FAMILY = cc13x0

    ### Add to the source dirs
    CONTIKI_TARGET_DIRS += launchpad/cc1350

    BOARD_SOURCEFILES += rf-switch.c tx-power-driver.c

    ### Include the common launchpad makefile
    include $(PLATFORM_ROOT_DIR)/launchpad/Makefile.launchpad


    This makefile is contained in this path : C:\cygwin64\home\user\contiki-ng-mtx\examples\platform-specific\cc26x0-cc13x0\190619_MTX_DOME -

    # File di configurazione del sistema
    DEFINES+=PROJECT_CONF_H=\"MTX_Config.h\"

    # Nome del progetto
    CONTIKI_PROJECT = MTX_DOME
    all: $(CONTIKI_PROJECT)
    PLATFORMS_ONLY = cc26x0-cc13x0

    # File Source da utilizzare
    PROJECT_SOURCEFILES += MTX_Coap.c
    PROJECT_SOURCEFILES += MTX_Debug.c

    ........

    .........

    .......

    CONTIKI_WITH_IPV6 = 1

    # REST Engine shall use Erbium CoAP implementation
    MODULES += er-coap
    MODULES += rest-engine
    MODULES += mqtt

    # Il percorso in cui e' presente il sistema operativo CONTIKI.
    CONTIKI = ../../..

    # Aggiunta del file Makefile.include al progetto in cui
    # sono presenti tutte le definizione del sistema operativo
    include $(CONTIKI)/Makefile.include

    But there is always a same problem: no rule to make a target.

    What am I wrong?

    best

    thanks in advance 

    I ll very appreciate your answer