Greetings,
I'm bringing up a CC1352P Rev E board design. While some of my boards are working well, I've got a few that reset upon receiving or transmitting a Sub1GHz packet. The System Reset from SySCtrlResetSourceGet() returns 0x5 which is CLK_LOSS. Both the 32kHz and 48kHz crystals on these boards look good on a scope. I've noticed Advisory Radio_02 High-Power PA Operation at Temperatures Below -20C May affect the 32-kHz Crystal Oscillator but I'm operating these at room temp. If I understand how to read the STAT0/STAT1 registers I get STAT0:0x665c0000 STAT1:0x000061e1.
Any ideas what can be going on here?
Regards,
Tim