Greetings,
I'm working with a custom CC1352P board which we program via JTAG and OpenOCD. I've found that our board which has no on-board antenna will reset with a reset cause of CLK_LOSS when a packet is transmitted with no antenna load. I've found that this hampers the ability to JTAG program the device - if for example I have something like the rfPacketTx example app running the board resets so quickly that I can't JTAG program it.
Two questions:
1. is there any way to avoid the resetting while transmitting with no antenna in our hardware design (other than the obvious of having an on-board antenna)
2. how can I JTAG program a device that is continually resetting itself?
Regards,
Tim