Other Parts Discussed in Thread: WMBUS, MSP430FR4133,
Hello,
I am interested in developing a 169 MHz Wireless M-Bus solution, but I need to understand the following before I make a decision, I will be grateful if you can provide me with answers:
1-) Is a free WMBUS Wireless M-Bus Protocol Software available for the two-chip solution of the MSP430 + CC112x and CC120x from TI - the WMBUS download seems to be for the CC13x0?
2-) If the answer to the question above is yes, are there any limitations to the stack (limited number of nodes, no source code, no support, etc.)?
3-) What is the development platform for this stack?
4-) Is there another free software stack provided by TI other than the WMBUS that can also be used to create a low-power star network with the same hardware - I am particularly interested in the 169 MHz?
Thanks in advance.