Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: CC1352P
Greetings,
I'm using the EasyLink from simplelink_cc13x2_26x2_sdk_3_20_00_68 with the CC1352P1_LAUNCHXL board and finding that any of the 2.4GHz modes are failing init. The AT command reference shows 'Error 0005' which doesn't quite make sense (EasyLink_Status_Tx_Error = 5). The other modes appear to work fine.
What I'm looking for is a way to test our CC1352P board in our production environment thus I want to ensure they can TX and RX both at 2.4GHz, and at Sub1GHz.
Thanks,
Tim