Other Parts Discussed in Thread: TIDA-010003, CC1310
Trying to implement mesh network by cc1310(node - TIDA-010003) & cc1310+Msp432(root - TIDA-01547)
First trying to to fully understand and implement node network. Referring to TIDA-010003, Fig 1 on page 2.
Please correct or suggest if anything need to be done differently in below points.
1. Refer to fig 1, need to select 863Mhz & long range mode 5, so in config.h , I have defined like this
#define CONFIG_PHY_ID (APIMAC_STD_US_915_PHY_1)
2. Need to use freq hoping mode. So this code in features.h
#undef FEATURE_ALL_MODES //FIXME
/*! If defined, builds the image with the frequency mode of operation */
#define FEATURE_FREQ_HOP_MODE //FIXME
/*! If defined, builds the image with beacon mode of operation */
#undef FEATURE_BEACON_MODE
/*! If defined, builds the image with non beacon mode of operation */
#undef FEATURE_NON_BEACON_MODE
3. In video series, it is mentioned that both parent and node should know the hopping pattern. i have mode node & root codes able to compile & build. Where this pattern is defined?
4. Have battery operated application, node send data only when interrupt occurs. So i thibk best option is debug_push_leaf. If any other options let me know?
5. Also Is debug_push_leaf is final release build also? Or we cna further reduce size/improve speed by release setting? If yes, what parameters in debug_push_leaf need to be undefined?
Have next queries also, but first help me to set these values in node code.