This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LAUNCHXL-CC1310: Doesn't wake up after few months

Prodigy 140 points

Replies: 13

Views: 239

Part Number: LAUNCHXL-CC1310

Hello everybody,

I've build a simple remote controller with 3 relay outputs around the CC1310 launchpads as prototype.

For the remote; the system is working around a 3V battery, current consumption is about 6µA when not in use.

The proto's are currently in use, and we are running into a problem which perhaps you can help me with. 

After a few months, 3 or so, the remote gets stuck. To explain myself better I'll explain the software flow:

using TIRTOS; CCS V7 and Windows 10.

I'll first create a task, the transmitPackageTask and a semaphore, configure the led and button pins, configure the interrupts for the buttons and configure the semaphore. Then call BIOS_start().

Now when a button is pressed, the callback will post the semaphore, which will enable the transmitPackageTask to run and send 5 packets with information about the button, batteryvoltage and temperature. After those are sent the semaphore will be pend and the CPU will goes back to sleep.

Has anybody an idea about the CPU getting stuck after a few months? I'll have to go there to measure things like battery voltage and stuff, but the battery was just new. 

/*
 * Copyright (c) 2015-2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*
 *  ======== Filled with transmitter code ======== 
*/
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/runtime/System.h>

/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>

/* TI-RTOS Header files */
#include <ti/drivers/PIN.h>
#include <driverlib/aon_batmon.h>
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>


/* Board Header files */
#include "Board.h"
#include "smartrf_settings/smartrf_settings.h"

#define TASKSTACKSIZE  1024
#define PAYLOAD_LENGTH      30

Task_Struct task0Struct;
Char task0Stack[TASKSTACKSIZE];

/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;
static PIN_Handle buttonPinHandle;
static PIN_State buttonPinState;

static RF_Object rfObject;
static RF_Handle rfHandle;

Semaphore_Struct semStruct;
Semaphore_Handle semaphore;

/*
 * Application LED pin configuration table:
 *   - All LEDs board LEDs are off.
 */
PIN_Config ledPinTable[] = {
    Board_LED0 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    Board_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    PIN_TERMINATE
};

PIN_Config buttonPinTable[] = {
    Board_BUTTON0  | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_NEGEDGE,
    Board_BUTTON1  | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_NEGEDGE,
    Board_BUTTON2  | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_NEGEDGE,
    PIN_TERMINATE
};


uint8_t butState = 0;

/*
 *  ======== heartBeatFxn ========
 *  Toggle the Board_LED0. The Task_sleep is determined by arg0 which
 *  is configured for the heartBeat Task instance.
 */
Void transmitPackageTask(UArg arg0, UArg arg1)
{
	uint8_t i;
	uint32_t bat_voltage;
	int32_t temp_deg_cel;
	uint8_t packet[PAYLOAD_LENGTH];
	RF_Params rfParams;
	RF_Params_init(&rfParams);

	RF_cmdPropTx.pktLen = PAYLOAD_LENGTH;
	RF_cmdPropTx.pPkt = packet;

	/* Reserved data for ID or something else in the future */
	packet[3] = (uint8_t) 0;
	packet[2] = (uint8_t) 0;
	packet[1] = (uint8_t) 0;
	packet[0] = (uint8_t) 0;

    while (1) {

    	Semaphore_pend(semaphore, BIOS_WAIT_FOREVER);

		/* Request access to the radio */
		rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);

		/* Set the frequency */
		RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
		if(AONBatMonNewBatteryMeasureReady() == 1){
			bat_voltage = AONBatMonBatteryVoltageGet();
		}

		if(AONBatMonNewTempMeasureReady() == 1){
			temp_deg_cel = AONBatMonTemperatureGetDegC();
		}

		packet[7] = (uint8_t)bat_voltage;									//CPU voltage (battery voltage / ADC voltage)
		packet[6] = (uint8_t)(bat_voltage >> 8);							//CPU voltage (battery voltage / ADC voltage)
		packet[5] = (uint8_t)(bat_voltage >> 16);
		packet[4] = (uint8_t)(bat_voltage >> 24);

		packet[12] = (uint8_t)temp_deg_cel;									//CPU voltage (battery voltage / ADC voltage)
		packet[11] = (uint8_t)(temp_deg_cel >> 8);							//CPU voltage (battery voltage / ADC voltage)
		packet[10] = (uint8_t)(temp_deg_cel >> 16);
		packet[9] = (uint8_t)(temp_deg_cel >> 24);

		packet[13] = butState;						//Buttons: b0 = pin 1, b1 = pin2, b2 = pin 3.....b7 = pin 8
		butState = 0;

		for(i = 0; i < 5; i++){
			/* Send packet */
			RF_EventMask result = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx, RF_PriorityNormal, NULL, 0);
			if (!(result & RF_EventLastCmdDone))
			{
				/* Error */
				while(1);
			}
		}
		PIN_setOutputValue(ledPinHandle, Board_LED0, 0);
		PIN_setOutputValue(ledPinHandle, Board_LED1, 0);
		RF_close(&rfObject);
    }
}

void buttonCallbackFxn(PIN_Handle handle, PIN_Id pinId) {
    /* Debounce logic, only toggle if the button is still pushed (low) */
    CPUdelay(8000*50);

    if (!PIN_getInputValue(pinId)) {
        /* Toggle LED based on the button pressed */
        switch (pinId) {
            case Board_BUTTON0:
                PIN_setOutputValue(ledPinHandle, Board_LED0, 1);
                butState |= 1;
                break;

            case Board_BUTTON1:
                PIN_setOutputValue(ledPinHandle, Board_LED1, 1);
                butState |= 2;
                break;
            case Board_BUTTON2:
                PIN_setOutputValue(ledPinHandle, Board_LED1, 1);
                PIN_setOutputValue(ledPinHandle, Board_LED0, 1);
                butState |= 4;
                break;
            default:
                /* Do nothing */
                break;
        }

        Semaphore_post(semaphore);
    }
}


/*
 *  ======== main ========
 */
int main(void)
{
    Task_Params taskParams;

    /* Call board init functions */
    Board_initGeneral();
    AONBatMonEnable();

    /* Construct heartBeat Task  thread */
    Task_Params_init(&taskParams);
    taskParams.arg0 = 1000000 / Clock_tickPeriod;
    taskParams.stackSize = TASKSTACKSIZE;
    taskParams.stack = &task0Stack;
    Task_construct(&task0Struct, (Task_FuncPtr)transmitPackageTask, &taskParams, NULL);

    Semaphore_Params semParams;

    /* Open LED pins */
    ledPinHandle = PIN_open(&ledPinState, ledPinTable);
    if(!ledPinHandle) {
        System_abort("Error initializing board LED pins\n");
    }

    buttonPinHandle = PIN_open(&buttonPinState, buttonPinTable);
	if(!buttonPinHandle) {
		System_abort("Error initializing button pins\n");
	}

	 /* Setup callback for button pins */
	if (PIN_registerIntCb(buttonPinHandle, &buttonCallbackFxn) != 0) {
		System_abort("Error registering button callback function");
	}


	Semaphore_Params_init(&semParams);
	Semaphore_construct(&semStruct, 0, &semParams);

	semaphore = Semaphore_handle(&semStruct);

    System_printf("Starting the example\nSystem provider is set to SysMin. "
                  "Halt the target to view any SysMin contents in ROV.\n");
    /* SysMin will only print to the console when you call flush or exit */
    System_flush();

    /* Start BIOS */
    BIOS_start();

    return (0);
}

  • Hey,

    This might sound like a crazy idea, but have you tried using the RTOS debug tools to check the state of the RTOS?

    You could be running out of heap or something. With the CCS RTOS tools, you can search the the stack status, and heap status. Maybe that's whats is causing your issues.

    -CE

  • Guru 269065 points

    In reply to Capricious Engineer:

    - First: Could you define what " remote gets stuck" means? If the remote is still stuck, you can try to attach a debugger "attach to running target" is an option and see where the code has stopped. 

    - I can think of the following reasons for the code to get stuck:

    - Memory: You have a memory leakage somewhere. Your code looks fine at the first glance. But I believe it should not be required to do RF_open within the while(1) but just do it once before the loop.

    - Timing: That a start of a function is set to the past or similar. I see that you use the clock module and that you have set arg0 to something but haven't looked into what it does. 

    - The code has got stuck in one of the while(1) error loops. 

    Second: Are you able to reproduce the "crash" in shorter time? If you have a testing code that emulate button push, do you then get stuck after a short time? 

    I would assume you should use less than 1 uA when you are not pressing anything. 

     

  • Guru 269065 points

    In reply to TER:

    Any update?

     

  • In reply to TER:

    Hello,

    Thanks for your replies. I haven't got the actual remote that is stuck, but I do have another remote lying here.


    To exclude the memory problems I figured I'd connect with ROV and try to analyse the memory for leaks or similair, but I can't get the ROV to connect… I keep getting a js error: js: "C:/ti/xdctools_3_32_00_06_core/packages/xdc/xdc.tci", line 354: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: can't locate the package 'xdc.rov.monserver' along the path: 'C:/ti/tirtos_cc13xx_cc26xx_2_21_01_08/packages;C:/ti/tirtos_cc13xx_cc26xx_2_21_01_08/products/tidrivers_cc13xx_cc26xx_2_21_01_01/packages;C:/ti/tirtos_cc13xx_cc26xx_2_21_01_08/products/bios_6_46_01_38/packages;C:/ti/tirtos_cc13xx_cc26xx_2_21_01_08/products/uia_2_01_00_01/packages;C:\ti\xdctools_3_32_00_06_core/packages;'. Ensure that the package path is set correctly.

    I think there are some version mismatches but I can't seem to figure out where. When I switch to the latest XDC tools version I can't compile because of sysbios.

    First I'll have to fix that before I can go further analysing the memory. I'll let you know when I'm getting further. 

    Greetings,

    Marcel

    P.S. Im using CCS 9.1.0. 

  • Guru 269065 points

    In reply to Marcel van den Heuvel:

    tirtos_cc13xx_cc26xx_2_21_01_08 is a few year old. SInce you have issues now, are you able to update to the latest SDK? 

     

  • Guru 269065 points

    In reply to TER:

    Any update? 

     

  • In reply to TER:

    Today I'm working to update the SDK. 

    I'll let you know when that is finished and how the memory usages are over a longer period of time and transmissions. 

    Thanks!

  • In reply to Marcel van den Heuvel:

    I've managed to re-create the software using the newer TIRTOS and XDC tools. These are the version I'm using from now on:

    TI-RTOS: 2.21.1.08

    XDCTools: 3.55.2.22

    They seem to work nice and now I can use the ROV. 

    But; I don't see anything growing in the memory. Free heap space stays at 0x1000 like there is nothing being malloc'ed. Also the stack peaks stay at around 50% of the given stack space for the tasks. I've uploaded an overview of the ROV dashboard. The transmitpackageTask is also nicely blocked by the semaphore as expected.

    Note: The yellow backgrounds I've added myself, not the ROV.

    Perhaps the best idea would be to give it a try with the tirtos being updated and see if this system still get stuck in a few months?

  • Hi,

    You use RF_close(&rfObject) - this should be RF_close(rfHandle).

    After RF_open you should check that rfHandle is not NULL.

    HC

  • Guru 269065 points

    In reply to Hans Christian Glittenberg:

    TI-RTOS: 2.21.1.08 is not the newest version. You should be using SimpleLink CC13x0 SDK (3.20.00.23)  dev.ti.com/.../node

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.