This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: TI 15.4 stack: Issue on the newest SDK

Part Number: CC1310

Hi TIs,

We use the newest SDK for our application, we met unnormal issue.

settings as follow:

SDK:Simplelink_cc13x0_sdk_3_20_00_23

Rate: 50kbps@433MHz

Collector: 1; sensor: 10

mode:beacon mode

IAR Version:8.32.1

#define CONFIG_MAC_BEACON_ORDER          8

#define CONFIG_MAC_SUPERFRAME_ORDER      8

After the Sensor is connected to collector for 10 minutes, Since the collector will be close.  the Sensor is always in the scanning state and cannot enter the orphan state.

If the sensor and collector are connected again and the collector is closed within a short time, the sensor can normally enter the orphan state. 

In the last SDK , we donot meet the issue. Because sensor always in the scanning state ,the system power dissipation cannot be  ensure.

Pls give recommendation on this issue.

Thanks a lot.

BR 

Sara