Other Parts Discussed in Thread: LAUNCHXL-CC1352P1, CC1352R, CC1352P
Dear Sir,
I would like to ask (only for sure) if the LPSTK-CC1352R is 100% compatible with the LaunchPads LAUNCHXL-CC1352P1, LAUNCHXL-CC1352P-2 to?
Best regards
Mira
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I would like to ask (only for sure) if the LPSTK-CC1352R is 100% compatible with the LaunchPads LAUNCHXL-CC1352P1, LAUNCHXL-CC1352P-2 to?
Best regards
Mira
Hi Mira,
LPSTK-CC1352R is based on the CC1352R device. So you can directly use an image compiled for CC1352R on it. However, you cannot directly use an image compiled for CC1352P (because CC1352P and CC1352R are not exactly exactly the same devices).
With that said, the code is easy to port from one device to the other.
I hope this will help,
Regards,