Good Afternoon,
We are implementing some of the equation explained in the CC1200 user's manual and Smart RF studio.
But if you select the first standard modulation (1.2kbs,2fsk,12.5Khz BW) you can see that the AGC_Reference value is 20h.
If you use the equations provided on RF studio, the results below 100Khz doesn't match with the equations!
This is the result expected by equation ---> RX filter BW AGC_REFERENCE 10 kHz 0x2F (MDMCFG1.DVGA_GAIN = 0, RSSI offset ≈ −99 dB)
This is the result given by the RF studio selecting the first setting (1.2kbs,2fsk,12.5Khz BW) --> [7:0] AGC_REFERENCE = 0x20
The same happend with the IFAMP_BW calculation.
This is the equation given on RF studio --- > Single Side BW > f_IF+(RX Filter BW/2)
If you load the standard setting ( 50Ksps, 2gfsk ieee 802.15.4g ) the RF studio gives IFAMP_BW = 01 ( 600Khz ) but if you apply the above equation, should be 300Khz.
But if test the system with two TI board CC120xEM 868/930(using the above settings) and using the RF studio parameter, you get (as expected) slightly worse result then using the value given by the equation. ( Less BW means less noise..)
Can you please check if the equations are correct and/or if the RF studio is calculating correctly the value?
Thank you,
Alex