Hello,
i have to do the programming through UART for the mass production. I have read the document based on that i do the connection. now for the programming i am using the cc1350 LP board.
I am using flash programmer 2 software for the UART programming. so my connection like this
DIO 2-->RX
DIO 3-->TX
and usb to serial connector connected to PC software. The required changes for the boot loader done in CCFG file of my application code.
#ifndef SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE
//#define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE 0x00 // Disable ROM boot loader
#define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE 0xC5 // Enable ROM boot loader
#endif
#ifndef SET_CCFG_BL_CONFIG_BL_LEVEL
// #define SET_CCFG_BL_CONFIG_BL_LEVEL 0x0 // Active low to open boot loader backdoor
#define SET_CCFG_BL_CONFIG_BL_LEVEL 0x1 // Active high to open boot loader backdoor
#endif
#ifndef SET_CCFG_BL_CONFIG_BL_PIN_NUMBER
#define SET_CCFG_BL_CONFIG_BL_PIN_NUMBER 0x07 // DIO number for boot loader backdoor
#endif
#ifndef SET_CCFG_BL_CONFIG_BL_ENABLE
#define SET_CCFG_BL_CONFIG_BL_ENABLE 0xC5 // Enabled boot loader backdoor
//#define SET_CCFG_BL_CONFIG_BL_ENABLE 0xFF // Disabled boot loader backdoor
#endif
after this setting i have browse that .out file into my flash programmer .after all this connection my device is connected. i am displaying image below.