I followed the instructions listed here only using version 2.10.00.12 of the SDK and version 06.01.00.08 of the BBB SD image. When I start run_demo.sh I get this
Launching the Collector Application in the background
Collector Running as Process id: 1038
Launching Node-JS gateway application in background
which: no nodejs in (/usr/local/bin:/usr/bin:/bin:/usr/local/sbin:/usr/sbin:/sbi
Gateway is running as Process id: 1048
Followed by this error that repeats every few seconds.
ERROR: Rcvd Error on the socket connection with AppServer
I have tried flashing the launchpad with both the .hex file in the Linux SDK as well as the example project in simplelink SDK 2_30_00_45 (due to chip rev being 1.1)
Any insight would be greatly appreciated.
Thank you