Other Parts Discussed in Thread: WMBUS,
I'm trying to run a simple test to check wMBus protocol.
To do so, I have CC1310 LaunchPad, and I installed the "wmbus_cc13x0_rtos_2_0_0.exe"
Then I loaded the Serial_CC13xx_Collector_T2.hex on CC1310 LaunchPad, and connected it to PC to test with.
I got the project of serial library swra466b/sblAppEx_1_03_00_00. When I run it and open the port of LaunchPad's UART I got an error and couldn't have wMBus protocol running!
The goal of my test is to check the protocol and test it, I have a wMBus water meter and I'll use the CC1310 LaunchPad as collector to read the meter, commuicating with CC1310 LaunchPad will be through the serial UART using sblAppEx_1_03_00_00, am I right?
Can you please help?