Other Parts Discussed in Thread: CC1310, CC1312R
Hello,
How i get the 6LoWPAN collector example for CC1310. I got the Sensor end node example code for the 6LoWPAN.
Thank You
Nilesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello nilesh,
We have two of them. If you prefer an embedded based one, look at this: http://www.ti.com/tool/TIDA-01547
If you prefer a linux based one, look at this: http://www.ti.com/tool/TIDA-010032
Regards,
AB
Hello,
The embeded one www.ti.com/.../TIDA-01547 is part implemented on cc1350(wireless+15.4) and part implemented on msp432(lowpan part). 1. Is it possible to port the entire project(tida-01547) to the cc1350(wireless+15.4+6lowpan)? 2. Can you give any instructions for the same? 3. Also is it possible to port the cc1310(www.ti.com/.../TIDA-010003) node project to cc1350 as collector project? 4. What is the major difference between www.ti.com/.../TIDA-010003 and www.ti.com/.../TIDA-010024 ?
Thank You
Nilesh
Hello Nilesh,
1. Some evaluation would need to be done, but most likely no. The main limitation here is memory.
2. Reduce as much code size as possible, but I do not think it will be possible.
3. a collector can also act as a sensor, you just need to understand how the apis work and call them in the required sequence.
4. One is last gen device (Core M3 and less memory) and the other in current gen device (Core M4F+ and more memory)
Regards,
AB
Hello,
As we know there is memory constraint while converting collector CC1312R code to CC1310. we are planning to change the collector side by CC1312R MCU.
and end node will be CC1310.
so my question is ,
1)How many number of end node(CC1310) i can connect to the CC1312R(collector) in a network?.
2) Is there any memory constraint for this network communication.?
So for the application i wiill use collector (CC1312R) source code with my custom application. for the end node(CC1310) i will use end node mesh example code.
Hello,
1) The number of nodes will be limited by the collector device's memory, in this case ~150 nodes.
2) The memory constraints will be on the collector side and how many nodes you connect to it.
Regards,
AB
Hello Nilesh,
I do not understand your question, the only memory constraint device will be the collector device. Each individual node will not have a problem with its memory since it will only be running its own application and not keeping track of anyone else like the collector does.
Regards,
AB
Hello,
Ok i got it. Just i am here change my track . In TI 15.4 Stack there is sensor and collector example . between this 2 devices the start topology is used here please correct me if i am wrong. so can i make this code in mesh topology by using this existing start protocol
also please provide me the sensor and collector example code documentation.
Thanks
Nilesh
HEllo,
Yes, collector and sensor use the star topology.
You can potentially add mesh on top of this, but will require some work.
Example documentation: http://dev.ti.com/tirex/explore/node?node=APeHcG.A0wniaym22zAYKw__pTTHBmu__LATEST
Sensor code: http://dev.ti.com/tirex/explore/node?node=ANxl4XDaphMk93voj1Kceg__pTTHBmu__LATEST
Collector code: http://dev.ti.com/tirex/explore/node?node=AN4THZ2vpN78bjmiszGJvw__pTTHBmu__LATEST
Regards,
AB