This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS/CC1101: CC1310 and CC1101 communication settings

Intellectual 340 points

Replies: 14

Views: 117

Part Number: CC1101

Tool/software: Code Composer Studio

Hi,

I use CC1310 and CC1101 modules in my project, but I could not communicate these two modules with each other.

The settings I use are as in the picture.

CC1101_SmartRF_Setting

CC1310_SmartRF_Setting

These are the settings I use, but I have not been able to operate with these settings yet.

1. 

I first tried communicating CC1101 settings with two CC1101s but failed.

These two modules communicate with CC1101 and 868 Mhz.
Its original settings are as follows.

/**
 * CC1101 configuration registers - Default values extracted from SmartRF Studio
 *
 * Configuration:
 *
 * Deviation = 20.629883 
 * Base frequency = 867.999939 
 * Carrier frequency = 867.999939 
 * Channel number = 0 
 * Carrier frequency = 867.999939 
 * Modulated = true 
 * Modulation format = GFSK 
 * Manchester enable = false
 * Data whitening = off
 * Sync word qualifier mode = 30/32 sync word bits detected 
 * Preamble count = 4 
 * Channel spacing = 199.951172 
 * Carrier frequency = 867.999939 
 * Data rate = 38.3835 Kbps
 * RX filter BW = 101.562500 
 * Data format = Normal mode 
 * Length config = Variable packet length mode. Packet length configured by the first byte after sync word 
 * CRC enable = true 
 * Packet length = 255 
 * Device address = 1 
 * Address config = Enable address check
 * Append status = Append two status bytes to the payload of the packet. The status bytes contain RSSI and
 * LQI values, as well as CRC OK
 * CRC autoflush = false 
 * PA ramping = false 
 * TX power = 12
 * GDO0 mode = Asserts when sync word has been sent / received, and de-asserts at the end of the packet.
 * In RX, the pin will also de-assert when a packet is discarded due to address or maximum length filtering
 * or when the radio enters RXFIFO_OVERFLOW state. In TX the pin will de-assert if the TX FIFO underflows
 * Settings optimized for low current consumption
 */
//#define CC1101_DEFVAL_IOCFG2     0x29        // GDO2 Output Pin Configuration
#define CC1101_DEFVAL_IOCFG2     0x2E        // GDO2 Output Pin Configuration
#define CC1101_DEFVAL_IOCFG1     0x2E        // GDO1 Output Pin Configuration
#define CC1101_DEFVAL_IOCFG0     0x06        // GDO0 Output Pin Configuration
#define CC1101_DEFVAL_FIFOTHR    0x07        // RX FIFO and TX FIFO Thresholds
#define CC1101_DEFVAL_SYNC1      0xB5        // Synchronization word, high byte
#define CC1101_DEFVAL_SYNC0      0x47        // Synchronization word, low byte
#define CC1101_DEFVAL_PKTLEN     0x3D        // Packet Length
#define CC1101_DEFVAL_PKTCTRL1   0x06        // Packet Automation Control
#define CC1101_DEFVAL_PKTCTRL0   0x05        // Packet Automation Control
#define CC1101_DEFVAL_ADDR       0xFF        // Device Address
#define CC1101_DEFVAL_CHANNR     0x00        // Channel Number
#define CC1101_DEFVAL_FSCTRL1    0x08        // Frequency Synthesizer Control
#define CC1101_DEFVAL_FSCTRL0    0x00        // Frequency Synthesizer Control
// Carrier frequency = 868 MHz
#define CC1101_DEFVAL_FREQ2_868  0x21        // Frequency Control Word, High Byte
#define CC1101_DEFVAL_FREQ1_868  0x62        // Frequency Control Word, Middle Byte
#define CC1101_DEFVAL_FREQ0_868  0x76        // Frequency Control Word, Low Byte
// Carrier frequency = 902 MHz
#define CC1101_DEFVAL_FREQ2_915  0x22        // Frequency Control Word, High Byte
#define CC1101_DEFVAL_FREQ1_915  0xB1        // Frequency Control Word, Middle Byte
#define CC1101_DEFVAL_FREQ0_915  0x3B        // Frequency Control Word, Low Byte
// Carrier frequency = 433 MHz
#define CC1101_DEFVAL_FREQ2_433  0x10        // Frequency Control Word, High Byte
#define CC1101_DEFVAL_FREQ1_433  0xA7        // Frequency Control Word, Middle Byte
#define CC1101_DEFVAL_FREQ0_433  0x62        // Frequency Control Word, Low Byte
#define CC1101_DEFVAL_MDMCFG4    0xCA        // Modem Configuration
#define CC1101_DEFVAL_MDMCFG3    0x83        // Modem Configuration
#define CC1101_DEFVAL_MDMCFG2    0x93        // Modem Configuration
#define CC1101_DEFVAL_MDMCFG1    0x22        // Modem Configuration
#define CC1101_DEFVAL_MDMCFG0    0xF8        // Modem Configuration
#define CC1101_DEFVAL_DEVIATN    0x35        // Modem Deviation Setting
#define CC1101_DEFVAL_MCSM2      0x07        // Main Radio Control State Machine Configuration
//#define CC1101_DEFVAL_MCSM1      0x30        // Main Radio Control State Machine Configuration
#define CC1101_DEFVAL_MCSM1      0x20        // Main Radio Control State Machine Configuration
#define CC1101_DEFVAL_MCSM0      0x18        // Main Radio Control State Machine Configuration
#define CC1101_DEFVAL_FOCCFG     0x16        // Frequency Offset Compensation Configuration
#define CC1101_DEFVAL_BSCFG      0x6C        // Bit Synchronization Configuration
#define CC1101_DEFVAL_AGCCTRL2   0x43        // AGC Control
#define CC1101_DEFVAL_AGCCTRL1   0x40        // AGC Control
#define CC1101_DEFVAL_AGCCTRL0   0x91        // AGC Control
#define CC1101_DEFVAL_WOREVT1    0x87        // High Byte Event0 Timeout
#define CC1101_DEFVAL_WOREVT0    0x6B        // Low Byte Event0 Timeout
#define CC1101_DEFVAL_WORCTRL    0xFB        // Wake On Radio Control
#define CC1101_DEFVAL_FREND1     0x56        // Front End RX Configuration
#define CC1101_DEFVAL_FREND0     0x10        // Front End TX Configuration
#define CC1101_DEFVAL_FSCAL3     0xE9        // Frequency Synthesizer Calibration
#define CC1101_DEFVAL_FSCAL2     0x2A        // Frequency Synthesizer Calibration
#define CC1101_DEFVAL_FSCAL1     0x00        // Frequency Synthesizer Calibration
#define CC1101_DEFVAL_FSCAL0     0x1F        // Frequency Synthesizer Calibration
#define CC1101_DEFVAL_RCCTRL1    0x41        // RC Oscillator Configuration
#define CC1101_DEFVAL_RCCTRL0    0x00        // RC Oscillator Configuration
#define CC1101_DEFVAL_FSTEST     0x59        // Frequency Synthesizer Calibration Control
#define CC1101_DEFVAL_PTEST      0x7F        // Production Test
#define CC1101_DEFVAL_AGCTEST    0x3F        // AGC Test
#define CC1101_DEFVAL_TEST2      0x81        // Various Test Settings
#define CC1101_DEFVAL_TEST1      0x35        // Various Test Settings
#define CC1101_DEFVAL_TEST0      0x09        // Various Test Settings
With these settings, two CC1101s communicate with each other.
2.
I have Tiva's own card, "TIDA-00489" sensor card, and I managed to communicate CC1310 launchpad with this card.
It communicates with 868 Mhz on two cards.
Now my question.
I am new to using these modules. Please can you tell me how to follow.
What I want to do is to get the sensor information from the "TIDA-00489" sensor card to CC1101 card.
There is an ATMEGA328P processor on the CC1101 board.
I tried the settings you suggested in the forum, but again it fails.
  • I can't connect when I play with these settings.I forgot to write
    #define CC1101_DEFVAL_MDMCFG4    0xCA        // Modem Configuration
    #define CC1101_DEFVAL_MDMCFG3    0x83        // Modem Configuration
    #define CC1101_DEFVAL_MDMCFG2    0x93        // Modem Configuration
    #define CC1101_DEFVAL_MDMCFG1    0x22        // Modem Configuration
    #define CC1101_DEFVAL_MDMCFG0    0xF8        // Modem Configuration
    Excel also marked different places between Standard CC1101 and the settings you and me suggested
  • Guru 262550 points

    In reply to Ali YOLCU:

    Please test with CMD_PROP_RADIO_DIV_SETUP.bBitReversal = 1 on CC1310. 

     

  • In reply to TER:

    It did not work.

    While the CC1310 is broadcasting, there is no change in the CC1101's GDO0 pin.

    When sending value between CC1101 and CC1101, there are changes in the pin.

    the arduino code i listen to is as below.

    attachInterrupt(CC1101Interrupt, messageReceived, FALLING);

  • Guru 262550 points

    In reply to Ali YOLCU:

    Before I sent the answer I checked with Studio and it worked, see attached for the cfg files. CC1101_OOK_E2E.xmlCC1310_OOK_E2E.xml

     

  • In reply to TER:

    I managed to read the value on CC1101 side. Thank you for your help.

    CC1101 side is having trouble reading the value continuously, it comes twice after it stops but it gets better when reset. It takes two values ​​and stops again. Why is this?

  • Guru 262550 points

    In reply to Ali YOLCU:

    Did it work when you use Studio? "CC1101 side is having trouble reading the value continuously": It's not clear what you mean here?

     

  • In reply to TER:

    Thank you Studio side worked.I solved the other question, no problem right now

  • In reply to TER:

    Sir, how did you get these CC1101 and CC1310 xml outputs?

    my settings are not working.

    can you send me an encrypted xml output For cc1101 and cc1310

  • Guru 262550 points

    In reply to Ali YOLCU:

    Sorry, could you elaborate? You wrote that you got the setting to work a few day back? 

    What do you mean by encrypted xml in this context? 

     

  • In reply to TER:

    2-I need a smartRF output to communicate with GFSK or GFSK.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.