Other Parts Discussed in Thread: CC1200
I am using CC1200 only as receiver (863-869MHz and 903 - 927MHz bands) and I use SmartStudio to setup registers.
I noticed that receiver can receive packets from small distance of transmitter (500mW) at wrong frequencies which are +40Mhz or -40Mhz.
What I want to say is that if transmitter sends packages at 863, I can receive it if receiver is set at 863 (expected) but also if I set it to 903Mhz (only a few meters from transmitter) and vice versa.
I have checked transmitter with spectrum analyzer and I can confirm there is no harmonics at +-40Mhz.
I have tried to find another distance instead 40MHz but didn't find. What is happening? That means that I will have trouble if someone is noising +-40Mhz from my central frequency.