• Resolved

CC1312R: txPower setting with boost mode

Expert 1155 points

Replies: 5

Views: 64

Part Number: CC1312R

Hi,

We are using CC1312R and boost mode (CCFG.c  setting to give VDDR1.95V.)

But the application can on the fly tune down output power in the code to 0 or even down to -10dBm

However the setting(txPower) we get from SmartRF studio and that is documenter in datasheet and in simplelink is based on the use of VDDR = 1.8V 

Do you have other smartRF studio setting for txPower valid for VDDR = 1.95V?

If not, how can we go about to find these values ourselves?

no-more-wires