Other Parts Discussed in Thread: ADS1231
CC1352P has internal DC to DC converter and its VDDS can be of the range of 1.8V to 3.6V. We are planning to connect non-rechargeable battery of 3V or 3.6V to as power input.
Internal DC-DC converter will generate VDDR which is of the range of 1.65 to 1.98 to power the RF section and digital section.
Kindly clarify below points.
1) Does VDDR also power the digital interface and i/o of CC1352P ?
2)All i/o and communication port of CC1352P is of logic voltage of 1.95V ? We may need to drive external MOS switch using i/o of SOC , what is your suggestion to increase the drive strength ?
3)ADS1231 VCC range is 3V to 5V and we are planning to power it by using 3.3V (TPS63031DSKR).
4)We are using AD 1231 which will be interfaced with CC1352P using SPI interface . We see there is I/O voltage level mismatch in interface. So do we need to use level translator for interfacing these ic ?