Tool/software: Code Composer Studio
Hey guys,
we use the latest SDK for CC1310 sensor/collector example in 15.4 stack. We have set our "max data retry" to 5, which works fine so far. According to the sniffer, the delay between the first send message (not acknowledged) and the retry send process is approximately 300ms (depending on the message length).
How is it possible to set the delay between retry send actions if a message was not acknowledged?
Is it correct, that the backoff exponents are only related to the LBT and CSMA channel scans prior to message transmission?
Is it possible to configure the application, that only data messages or data requests from the sensor are retried, but not disassociation notifications?
best wishes
Slev1n