Hi,
I have using cc1101 on our products, and debug it, today i fund a problem with it.
The same code, same drivers, power by usb, it's work fine, but failed on battery power.
The battery is two AAA batteries connected in series with a voltage of 2.57 volts.
When set receive mode, the marcstate register will be 0x08, and then, its be camed 0x00, always it!
I monitor marcstate register:
Init cc11xx...
No.1 marcstate: 01
Part:00
Ver:14
Config CC1101 with:
Addr: ab
ISM : 2
Mode: 1
Chn : 01
PAmp: 10
No.2 marcstate: 01
No.3 marcstate: 01
No.4 marcstate: 01
No.5 marcstate: 08
No.6 marcstate: 00
No.6 marcstate: 00
No.6 marcstate: 00