Other Parts Discussed in Thread: CC1101, CC-DEBUGGER, CC1310
I've built up a couple test boards for the CC1150 based around the provided 433MHz schematic.
The first one I built connected no problem and I could talk to it as I pleased while trying to figure out what my next step was in creating a Tx to Rx system.
But each of the following 2 boards I built when booted up came up with an "Invalid RF State on Startup" error when connecting to the SmartRF Studio 7. And after power cycling, neither board are recognized by the CC-Bugger.
When I went back to the first board I built it gave me the same error and the same results after a power cycle.
Notes on my setup:
I'm using a bench supply set for ~3.2V (verified with a voltmeter)
The debugger is plugged into my laptop
The testing above was spread out over a couple of days
As per the new normal, I am working from home, so I'm setup in my basement if that could affect anything.
Can anyone suggest ways forward?
Attached are the schematic and the board layout I've done up.
- It's already been brought to my attention that I swapped pins 10 and 11, this was corrected with cutting the traces and fly wiring to the closest contact point.