Part Number: CC1312R
Other Parts Discussed in Thread: SYSCONFIG, CC1310
Hi team,
Customer use CC1312+SKY66122 PA. How to enable PA ? by SysConfig or compile option ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Jerry,
Please see the following thread: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/827042?CCS-CC1312R-About-enabling-CC1190-by-define-CONFIG-RANGE-EXT-MODE
Unfortunately the files have been removed from the project and is not configurable via SysConfig. I would recommend importing the files from the CC1310 version and verify that the pins mapped are the ones in your configuration. The pin initialization code is in board_palna.c.
Normally the challenge in supporting Skyworks PA the control logic is different. So mapping the LNA_EN and PA_EN from the RFC is not enough.
Ref RC1882HPCF and RC1892HPCF from Radiocrafts that uses CC1312+ SAW + PA. www.radiocrafts.com
Solution is to map PA_EN out to GPIO to control PA/ /not LNA) signal on extern PA and then use global RFC interrupt to turn on PA chip (wake up from sleep)
whenever the RF core is turned on/off.
-no more wires