Hi,
We have linux gateways with a cc1310 co-processor mini-pci card. Somtimes the collector hangs with "ERROR: **ERROR** Set/Operation failed with status code: 0x19"
176342.202: reset-indication msg(1eab00) nbytes=11 len=6 [ 0xfe 0x06 0x41 0x80 0x04 0x03 0x01 0x02]
381901.064: Reset Indication: reason: 4 (rtos-assert) version: 3/1/2/2/0
381901.064: reset-indication msg(461152) nbytes=11 len=6 [ 0xfe 0x06 0x41 0x80 0x04 0x03 0x01 0x02]
439948.880: Reset Indication: reason: 4 (rtos-assert) version: 3/1/2/2/0
439948.880: reset-indication msg(506a3b) nbytes=11 len=6 [ 0xfe 0x06 0x41 0x80 0x04 0x03 0x01 0x02]
466405.808: Reset Indication: reason: 4 (rtos-assert) version: 3/1/2/2/0
466405.808: reset-indication msg(550b80) nbytes=11 len=6 [ 0xfe 0x06 0x41 0x80 0x04 0x03 0x01 0x02]
635124.399: Reset Indication: reason: 4 (rtos-assert) version: 3/1/2/2/0
635124.399: reset-indication msg(7273c4) nbytes=11 len=6 [ 0xfe 0x06 0x41 0x80 0x04 0x03 0x01 0x02]
683372.924: ERROR: **ERROR** Set/Operation failed with status code: 0x19
When restarting the collector we get the following error:
No reset response received after device reset
And we have to reboot the gateway to get it working again.
Searching for the error in the code has no results. What could be happening and where could I find the error codes?