Part Number: LAUNCHXL-CC13-90
Other Parts Discussed in Thread: CC1310, , LAUNCHXL-CC1310, CC1190, WMBUS
Hi,
We developed a project on the LAUNCHXL-CC1310 development kit and then designed our custom board based on the CC1310. Now we want to use the same project on the LAUNCHXL-CC13-90 development kit. After that, we will also design our custom board and program it.
I was wondering if we need to change anything in our software to adapt to this change? In the Smart RF Studio, when I connect to the LAUNCHXL-CC13-90 and try to use the config file saved for LAUNCHXL-CC1310, I get an error regarding mismatched parameters. I guess it is related to transmit power because the options in the transmit power are different in these kits.
So I wondered what kind of changes should I do on my project to migrate it to LAUNCHXL-CC13-90 design. Is there anything needs to be done in order to activate the amplifier for example?
Thanks,
Abdullah.